Hi everyone
What is the range and maximum speed I can measure using AWR1843BOOST?
I've done some experiments using the mmwaveSensingEstimator;
Max Range: 40m
Range Resolution: 150 cm
Max Velocity: 125
When I set the shape I got the following result.