This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSS4440: vs. PGA460

Part Number: TUSS4440
Other Parts Discussed in Thread: PGA460, TUSS4470

Hi,

Customers are considering the TUSS4440 or PGA460 for liquid level detection applications, but when comparing D/S, there seems to be no difference in functionality.

The TUSS4440 is expensive, is there any difference?

The PGA460 has a 12-bit ADC and temperature sensor, but it is lower cost.

However, if the TUSS4440 has advantages, it can be used even if it is expensive.

Is the TUSS4440 transducer driver better than the PGA460?

I need to clarify the difference between the two products according to the customer's request.

Best Regards,

Hiroshi

顧客はTUSS4440またはPGA460を検討していますが、D/Sを見比べても機能に差は無いように見えます。TUSS4440は高価ですが、何か違いがあるのでしょうか?PGA460は12bitADCと温度センサーを持っていますがより安価です。しかし、TUSS4440に利点があれば高価でも使用する可能性があります。
TUSS4440のトランスデューサードライバーはPGA460より優れていますか?
奇妙な質問で恐縮です。