Part Number: OPT301
I wonder if I can have a graph of the output voltage of the device vs constant IR light for OPT301 device. I'm using OP233 IR emitter with 10mA IF. OPR301 is powered with +/-5V. The output of the OPT301 was saturating so a paper filter was used to reduce the intensity of the light. I can now measure 0.8V out of the OPT301. But the issue is it is drifting a lot. Any recommendation on how to get constant output out of OPT301? What is the specification of the outptut voltage vs constant IR light? Ideally, it should be constant.
Thanks
Anuja