This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: About the SPI bootloader of IWR6843

Part Number: IWR6843


Hi Ti experts,

 

I want to design a new application with IWR6843 and STM32F103 MCU. The topology of this new design is that connect the MCU SPI interface to IWR6843’s SPI interface, meanwhile keep the QSPI interface from connecting to a QSPI FLASH, so the bootloader of IWR6843 master subsystem will load user’s firmware from the SPI path connected to MCU. Is there any demo or example of this application available? I want to know the more details of the data exchanging at SPI bus, could you give me some advices? 

 

Regards