Part Number: IWR6843
Hi,
While I understand that the demos in the ‘ti\mmwave_industrial_toolbox_4_5_1\labs’ are provided as is and there is minimal or no support, I still need to ask about errors arising when I try to run the MATLAB Runtime applications or .exe files.
Typical error is as in the image stating that “The ordinal 4739 could not be located in the dynamic link library…”.
I have tried to open the Visualizer apps for gesture, area scanner and people counting labs. I did this on three different (Windows 10) PCs and all returned this same error. On two of this PCs I can confirm that there were no problems till today and all apps worked well. One PC is a new/fresh installation of the apps, MATLAB and all procedures provided by Texas Instruments.
Not certain when last I updated my Windows OS on these PCs and I am wondering if there could be any correlation or this is a known error. At this stage however, it will be difficult to revert Windows updates Any other suggestions please?