Hi Ti Team,
We are looking for a sensor that will give an alarm near a high voltage, such an application scenario;The application platform is MTK6762, and the product is a smart wearing helmet.,For the following
High voltage near alarm with shock prevention warning function: when you wear near alarm and mistakenly into the live area (or will be into the live body, with pole) to a certain distance, near alarm can send out continuous alarm sound, remind you to pay attention to the danger of the live body.When you hear the alarm sound, you should quickly away from the high voltage live area, until the near alarm stops the alarm sound.The near alarm of this anti-electric shock warning function (also known as: near electric alarm function), can prevent due to the illusion and error caused by electric shock casualties.The low voltage of the near alarm has the function of electrical inspection: it can be used to detect whether there is electricity in the fire wire of more than 110V AC without touching the wire.Or used for cable and low voltage wire broken contact detection.Or for checking the direction of the wire in the wall of the user who stole electricity.Nearby alarm is an ideal warning auxiliary safety tool for high voltage electric power workers.