This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: TIDEP-01012 (Cascade Radar): Acquisition without Doppler

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: TIDEP-01012,

Hi,

Good day. I hope you are well.

Our customer has been using the TIDEP-01012 (MMWCAS-RF-EVM) and they have an inquiry about it. I've copied it below. I hope you could help us with this.

One year ago, we received a TIDEP-01012 which we evaluated in the past year in various experiments for Structural Health Monitoring, and we are thrilled with the results. Until now, we always had to use at least 16 chirps per loop (min. requirement for DopplerFFT) however, we are actually not interested in velocity information and only want plain rangeFFTs to calculate interferograms. As we want as many acquisitions and as fast as possible acquire these interferograms (preferably up to 1000Hz), we would like to not use the DopplerFFTs and only receive rangeFFTs. However, the provided MatLab code is quite large and nested. I was wondering if there is already an existing solution of data processing with only one or two chirps per loop to increase the speed of acquisitions.

Looking forward to your support. Thank you.


Regards,

Cedrick

  • Hi,

    The post processing matlab scripts would need to be modified for this use case.

    We are not aware of an existing solution.

    I would have to open this question to the forum for more feedback.

    Thank you

    Cesar