Hi,
Is it possible to use gtrack sample code (6843) for other MCU or CPU (e.g., 1243 or 2243)?
If yes, how to do the modification or are there any related documents?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Silvia,
It should be possible to run this algorithm on an external CPU with the 2243. Please see the documentation for implementing the gtrack algorithm at the link below. (note the toolbox version may be different than below). You will need the pointcloud data as an input to the tracker as is, so you will need to generate this info.
C:/ti/mmwave_industrial_toolbox_4_6_0/labs/common/src/alg/gtrack/docs/doxygen3D/html/index.html
Additionally, please see the following training on the full processing chain for the SDK components used by gtrack.
Regards,
Jackson
Hi Silvia,
In general, the gtrack algorithm can be ported to any processor, but there may be significant effort in switching processors, or out of an embedded environment into a Linux environment. Certainly possible as long as you have the point cloud data as an input, but the memory allocation and other embedded specific commands will need to be updated.
Regards,
Jackson
Hi Silvia,
We do not have any specific guidelines on porting the algorithm to other processors, except what is given in the documentation about the function of the algorithm above and on the TI Resource Explorer.
Regards,
Jackson