This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA300: PGA300 DAC Calibration

Part Number: PGA300

PGA300, 4 to 20 mA mode, DAC Code Calibration:

When read and write DAC code

1) when 4 mA, reading was always very close to 4 mA

2) when 12 mA, reading was always very close to 12 mA

3) when 20 mA, sometime reading in amp meter was around 16 mA, even 5 mA. Recently this happened to one system with PGA300EVM-034. when tried later, some PGA300 can go back around 20 mA, some never made it.

Please help.