Other Parts Discussed in Thread: AWR1843
Hi expert,
We recentely bought two sets of AWR1843 + DCA1000EVM development kits. And One of the kits works well but the other seems like had harware failure.
To be specific, after installation of the development kits and 5v 2.5a power supplied , there was no led signal shown on AWR 1843 and in the mean time DCA1000 only had one 5v led light on. We tried to switch the DCA1000 for two kits seperately and confirmed the problem was from one of the DCA1000.
With the help of our tech assistant, we did some voltage and resistance tests as following. We think that one of our DCA1000 has hardware failure and hope we can get it exchanged. Please help us confirmed whether we had a hard ware failure on our DCA1000.
Thanks as always!
Test Signal |
Test |
Resistance to ground(Ω) |
Voltage to ground(V) |
Comments |
VCC_1V1(Or VCC_CORE) |
FL2 |
0.5 |
0.02 |
1.1V FOR FPGA_CORE_SUPPLY |
DDR_1V35(Or 1V35) |
FL3 |
267.3 |
1.292 |
1.35V FOR DDR3 |
3V3_A(3V3) |
FL4 |
25.6 |
1.5 |
3.3V FOR IO_SUPPLY |
2V5 |
FL1 |
2 |
1.2 |
2.5V FOR ETHERNET & 1.1V LDO_IN |
1V1 |
FL6 |
4.9 |
0.013 |
1.1V Ethernet PHY |
VCCHTX |
FL5 |
4.6 |
0.014 |
1.1V FPGA_SERDES |
5V |
FL8 |
450 |
2.45 |
POWER |
FL9 |
1.6 |
1.2 |