This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: No COM ports being shown in device manager

Part Number: IWR1642BOOST

Hello all,

I have powered on the Board using a 5V / 2.5A adapter and I see the LED blinking on the board. Please let me know if it is expected?

Upon connecting the device, in the device manager, I am unable to see the COM ports. I have installed all the required software. Below is the snapshot indicating the software installed.

Again trying to run drivers installation from C:\ti\xds110\drivers DPInst64.exe file, I am getting the following error.

Please let me know, how can I resolve this issue.

Thanks and Regards

Anirudh