Hi, the demo documentation says:
The purpose of the search window is to allow the test environment from not being overly constrained say because it may not be possible to clear it of all reflectors that may be stronger than the one used for calibration. The window size is recommended to be at least the distance equivalent of a few range bins. One range bin for the calibration profile (profile_calibration.cfg) is about 5 cm.
when I generate the .cfg file from the demo visualizer the default values for measureRangeBiasAndRxChanPhase are:
0 1.5 0.2
so, the search window is 0.2, it means, 20cm, is this search window valid for any target size or it depends of the target used?
Thanks