Part Number: TMAG5170EVM
Hi all,
playing with the EVM, i allow myself suggest to add some GUI functionnalities to enjoy the capability of the TMAG5170.
1/ to define a fix range, because when playing with the magnet, the range is always changing and it is difficult to understand the movement the magnet do
2/ to add a low pass or averaging filter, in order to improve the reading precision (equal to cancel the noise)
These shloud be much appreciated.
Thank you in advance.
Best regards.