Other Parts Discussed in Thread: PGA460
Hello.
I would like to calculate BPF coefficients to use unique BPF in PGA460-Q1.
Can you tell me about the following questions?
1.
I calculated BPF coefficients A2, A3 and B1 from the filter center frequency and the bandwidth with refference to this page.
However, the register value in PGA-460 and the result using the formula in the page did not match completely.
For example, if Bandwidth is 8kHz,
A3 = -399.3*Bandwidth+65512 = 1609.6
However, The register value was 1607(register value : 0x0647).
Is this difference due to the digit loss?
And, I presume A2, B1 are signed 16-bit, A3 is an unsigned 16bit. Is that correct?
2.
Is the BPF filter(second-order Butterworth IIR type) used in PGA460-Q1 the following transfer function?
( a2, a3 and b1 correspond to BPF coefficients A2, A3 and B1 respectively.)