This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: MRR Beam Steering Lab for MRR and USRR

Part Number: AWR1843BOOST


Hello,

Thanks for giving the MRR Beam Steering example for exploring more features of TI mmWave Radar. 

I have two quick questions.

(1) Was the Beam Steering feature applied for both MRR frame and USRR frame? Because I only want to use the USRR frame for my application, like "#define SUBFRAME_CONF_USRR", in default, will be the Beam Steering applied to the USRR?

(2) Because I only use the USRR, I guess it will save some cycles from the MRR. I want to recalculate the frame duration of the USRR, how can I do it? In the default example, which includes both MRR and USRR, the frame duration was 60ms. If I only use USRR, how to measure the new frame duration?

Thank you very much for the help!

Best,

Hang