Part Number: PGA305EVM-034
Hello Team,
My customer is trying to perform a calibration according to the attached data, however he was not successful.
data_calibration.zip
They did the DAC calibrations and 3P-1T reading, but when they are going to do the DAC readings it corresponds to the sensor reading, the fixed output is fixed at 0.34V. Where there should be a variation from 2.00 to 6.00V, according to the DAC calibration.
What could be wrong with this procedure?
Regards,
Renan