This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Baseband bandwidth and ADC sampling rate

Part Number: AWR1243

Hello,

We are using the AWR1243 in complex 1x mode, with the ADC sampling rate programmed to 18.75MHz. I see also that the analog baseband has a bandwidth of 15MHz. When I operate at ADC sampling rate of 18.75MHz, does this mean that any frequency content between 15 and 18.75MHz should be assumed to be noise and discarded? What are the recommended settings for ADC sampling rate?

Thanks for your help.

Best,
Antonio