This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2022: More information about the temperature accuracy

Part Number: HDC2022


In page 8 of the spec. sheet, there is only a temperature accuracy in typical value. And in page 5, the temperature accuracy in 5°C ≤ TA ≤ 60°C, is TYP +-0.2% and MAX +-0.7%. Do you have an MAX accuracy information in full working range? Could you show it in the figure as the figure in page 8.