Hi,
I have downloaded the GUI Software from the link provided and installed it as per the TDC1000-TDC7200EVM user guide.
1. The Tank level in GUI application in not being changed whenever the water level is being changed in the test cell but the TOF AVG and TOF STDEV are being varied.
2. Checked in device errors in the TDC1000TDC7200EVM user guide, it was mentioned that the port name in device manager must be TDC1000_7200_EVM if it is displaying as "MSP430-USBExample" we need to need to update the driver software. My PC is displaying the port name as USB Serial Device(COM41). Do I need to still update the driver software ?
Regards,
Hari Charan.