This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: MMWCAS-RF-EVM&MMWCAS-DSP-EVM control by Raspberry Pi4

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: MMWCAS-DSP-EVM, , AWR1243

Dear Team 

Good day

Our customer use the MMWCAS-RF-EVM&MMWCAS-DSP-EVM in their application , they want to confirm that , does they can use the Raspberry Pi4 to control and data exchange with the MMWCAS EVM?

If yes , could you provide any reference information to them ?

Best regards,

 Leon.liu

  • Hi,

    Could you please provide more detail about what you mean by "to control and data exchange with the MMWCAS EVM"?

    Do you have in mind to replace the MMWCAS-DSP-EVM board with a Rasberry Pi4?

    Thank you

    Cesar

  • Hi 

    Yes, they consider about whether the  Rasberry Pi4 can replace the  MMWCAS-DSP-EVM, they want to receive the raw Antenna data from RF board  and save the data in the Rasberry Pi4 TF card , then they will read the data from TF card and deal it with their own algorithm . this is first step , not real time data processing  . 

    By the way , for this application , they want to confirm that the signal from RF board . is the raw Antenna data, right ? just be convert to digital signal via AWR1243 , right ?

     

    They want confirm one more query ,  use MMWCAS-RF-EVM +MMWCAS-DSP-EVM to achieve real-time data processing ,they want to use 2 Rasberry Pi4 ,one connect to  MMWCAS-DSP-EVM via USB or Ethernet or any available interface, use  Rasberry Pi4 to control and receive the processed data from MMWCAS-DSP-EVM , another Rasberry Pi4  will remote control it and send the order or receive the data to image it .

    Best regards

    Leon.liu

     

  • Hi 

    Yes, they consider about whether the  Rasberry Pi4 can replace the  MMWCAS-DSP-EVM, they want to receive the raw Antenna data from RF board  and save the data in the Rasberry Pi4 TF card , then they will read the data from TF card and deal it with their own algorithm . this is first step , not real time data processing  . 

    By the way , for this application , they want to confirm that the signal from RF board . is the raw Antenna data, right ? just be convert to digital signal via AWR1243 , right ?

     

    They want confirm one more query ,  use MMWCAS-RF-EVM +MMWCAS-DSP-EVM to achieve real-time data processing ,they want to use 2 Rasberry Pi4 ,one connect to  MMWCAS-DSP-EVM via USB or Ethernet or any available interface, use  Rasberry Pi4 to control and receive the processed data from MMWCAS-DSP-EVM , another Rasberry Pi4  will remote control it and send the order or receive the data to image it .

    Best regards

    Leon.liu

  • Hi,

    The sensor will send the digital raw data through CSI-2 interface.

    Does the Rasberry Pi4 support a CSI2 interface?

    thank you

    Cesar