Dear team,
Can our device support 0.01k resolution?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
Can our device support 0.01k resolution?
Thanks & Best Regards,
Sherry
Hi Sherry,
Thank you for posting on our e2e forum. I'll have to know about his application to answer specifically.
The TMP61-Q1, along with other thermistors, are discrete devices. Most commonly used in a voltage divider they produce an analog output voltage that is typically fed into an ADC and translated into a temperature measurement. There is no direct relation between the thermistor and a 0.01K resolution.
In a typical voltage divider configuration, if we are to convert the analog voltage to a temperature range of -40 to 125C (165 steps) the voltage response comes out to 8mV/°K. Is this the figure you are looking for?
The resolution is dependent on the ADC. We recommend at least a 12 bit ADC for converting the analog output to temperature measurements.
Jalen