This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: EVM with single chip microcomputers

Part Number: IWR6843
Other Parts Discussed in Thread: MMWAVEICBOOST

Hi,

I was wondering if it will be possible to connect/control my IWR6843EVM and the MMWAVEICBOOST card from the GPIOs of a single chip microcomputer such as the Raspberry Pi or Arduino board. I am interested in toggling SPOs and capturing data on UART/SPI pins of the Boost card with connections to the microcomputer.

I understand from the MMWAVEICBOOST handbook that there is an interface on the J5 and J6 headers but not so clear on the use of the TI Launchpad. Could you please explain how this connection can be setup? What is the use of the Launchpad (which I understand to be another breakout board)?

I did try out the use of simple jumper wires to connect the UART pins on the Boost card (on J5.5, J5.7 and J5.4) to the UART on a Raspberry Pi, but could not get to send or receive any data from the connections. I was using pyserial library on Raspberry Pi and not sure if TI provided any library for any of these devices.

Looking forward to your guide and assistance.

-Tosin