This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA460PSM-EVM: PGA460 in a bi-static mode for a short range application ranging from 50mm to 1000mm.

Part Number: PGA460PSM-EVM
Other Parts Discussed in Thread: PGA460

Hello,

I am interested in using 30KHz to 80KHz transducers in a bi-static mode using a PGA460. I don't want to use higher frequency transducers since they tend to be expensive.  I also need them to be sealed.  I am looking for object detection in a  50mm to 1,000mm range.  The resolution can be 10mm.

I s this possible?  Am I being too optimistic here?