Other Parts Discussed in Thread: MMWAVEICBOOST


Hello
i am using IWR6843AOPEVM as standalone board for the
1)Human Vital's measurement
2)Multi Gesture Control
And the below image is the error i am receiving.
ERRORS:-
The COM ports doesn't tend to detect automatically and the USER PORT did not open, sensor stops instantly and the board doesn't seem to get any inputs from the radar.
QSERIAL PORT :- DEVICE NOT OPEN
note:- I am using this board in standalone mode and the board has been flashed with the pre-built binaries which is available in the industrial toolbox.
kindly help me fix the errors and i am only using the USB cable that is provided with the kit and I haven't powered the other USB socket for high power applications.
Thanks in advance Experts
Head's Up:-
The board works perfectly for flashing the pre-binaries and the only issue is that I cant get the board to Run the human vitals GUI nor the Multi gesture control GUI.
Akash Gondalia Mr.Akash i would be happy if You can hep me out. Thanks in Advance