Part Number: MMWAVE-STUDIO
Other Parts Discussed in Thread: IWR1443BOOST, DCA1000EVM
Hi Sir,
A customer has a installation issue on mmWaveStudio,
can you take some time to review it and give me valuable suggestions?
I'll summarize the problems of mmwave studio and send them to you.
In terms of hardware,
I am connecting IWR1443BOOST to PC by USB.
PC OS uses Windows 10 home 64 bit.
After installing and starting mmwave studio in this state,
The error shown in the attachment below occurred.
Please see the attachment ("mmwave studio") err.pdf “)
mmwave_studio_err.pdf
&&&&&&&&&&&&&&&
****Script FAILED!****
&&&&&&&&&&&&&&
Exception message is:
DLL' RadarLinkDLL.dll ' cannot be read: the specified module is not found.
(HRESULT exception: 0x8007007E)
In addition, Please see the attachment below after I confirmed the status of the current USB port in the PC device manager.
Please see the attachment ("USB" err.pdf “)
USB_err.pdf
"Texas Instruments debug probes" was not displayed at the beginning
Only one of "XDS 110 class auxiliary data port" exists under "other ports".
Yesterday, "mmwave studio" was installed to "matlab runtime (R22021a 32bit)" and "Visual C + + 2013 (32bit)" and then reinstalled,
It's the present status now.
(I also refer to the answer example of TI company in the failure case)
However, it is still attachment 1 "mmwave studio" err.pdf Abnormal state of.
Next step, I wanna connect "DCA 1000EVM",
Because I want to do the measurement experiment of sending and receiving。
Please confirm it for me。
Thanks a lot.