Other Parts Discussed in Thread: LM70, LM75B, LM73
Hi Sir,
May I know the heat flow used on LM75A which pin-out?
Temperature sensors: PCB guide lines for surface mount devices: https://www.ti.com/lit/an/snoa967a/snoa967a.pdf

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
May I know the heat flow used on LM75A which pin-out?
Temperature sensors: PCB guide lines for surface mount devices: https://www.ti.com/lit/an/snoa967a/snoa967a.pdf

Hi Henry,
May you clarify the heat flow you are interested in?
The application note linked in the original post here: https://www.ti.com/lit/an/snoa967a/snoa967a.pdf, explains the main paths for heat transfer on ICs (section 1.2) and provides visual examples of this heat transfer for separate packages with later figures. The LM75A is available in SOIC and VSSOP packages, so the primary path for heat transfer will be through the leads.
The same app note will provide suggestions on PCB design for ambient air temperature sensing which is best when thermally isolated from heat-producing devices on the same PCB.
Thank you,
Chris
Hi Sir,
My customer also asks questions as below.
1. Does the LM75A all pin-out can support detecting temperature?
2. The TOS and THYST min temp value is 80C and 75C? can be set to negative temp value?
3. Need or not to do the calibrate? how to get the relative temperature? need to set the relative temp value on a different type of environment?
4. The LM75A folder has shown to get the UL recognized. may I know it pass those UL certifications?
Dear Henry -
Sorry for the delay.
1. Yes, as Chris said, the leads of this device are primary path.
2. TOS default value is 80C, THYST default value is 75C, that is correct. These are two's complement based registers with 9 bits, so yes, it would seem they can be set to a negative value.
3. The devices will meet datasheet specs as shipped. Further calibration depends on your board and your requirements as to whether additional efforts are needed.
4. Digital sensors that are UL recognized in this family are the LM75B and LM75C. Additional devices are the LM73 and LM70 parts
Dear Henry -
The UL category for these UL recognized sensors is XAPX2. (for Temperature Indicating and Regulating Equipment)
According to the UL Product IQ website, they applied UL873 to these parts when testing.
File # is E232195