I am connecting the TMP431 to a diode-connected PNP transistor inside an ASIC device I want to monitor. The attached file shows the connections (my design does not use the optional resistors and capacitor so there is a direct connection). The attached file also contains a typical plot of temperature vs time that I see as the ambient temperature is raised, showing the remote (green) and local (brown) temperatures reported by the TMP431 along with a heatsink temperature (blue). The remote temperature reading should track the local temperature curve but with a relatively fixed positive offset. However the remote temperature readings take off at a higher rate and end up maxing out the extended range (the ASIC datasheet says we need to subtract 24C from the remote reading, so the resulting max is 167C). So the bottom line is that the local temperature readings are good but I don't know what is happening to the remote readings. Do you have any ideas on what might be going on here?TMP431 Remote Sensing.pdf