Hi,
Were trying to get mmWaveStudio running. We're using Window 10, mmWaveStudio mmwave_studio_02_01_01_00 with a AWR1843BOOST.
We followed all the instructions in the user guide, but get the following error? We followed the steps listed in a couple different E2E forum posts to no avail.
Q1. Is it required to have the DCA1000 hooked up or can we use mmWaveStudio with AWR1843BOOST standalone?
GM: Constructor
GM: Wed Mar 31 14:36:59 2021
RSTD.Transmit("/Settings")
[14:36:59]
[14:36:59] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[14:36:59] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[14:36:59] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[14:36:59] Scripter ignored: Attempt to UnBuild() again or before Build.
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[14:36:59] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[14:36:59] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[14:36:59] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[14:36:59] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[14:36:59] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[14:36:59] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[14:36:59] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[14:36:59] RSTD.Transmit("/")
[14:36:59] RSTD.SaveSettings(): Settings saved to "bla"
[14:36:59] RSTD.Build()
[14:36:59] RSTD.SaveSettings(): Settings saved to "bla"
[14:36:59] RSTD.Transmit("/")
[14:36:59] RSTD.AL_Build()
[14:36:59] RSTD.AL_LoadXml()
[14:36:59] RSTD.Transmit("/")
[14:36:59] RSTD.AL_Init()
[14:36:59] RSTD.Clients_Build()
[14:36:59] GM: Init
[14:36:59] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[14:36:59] GM: 1 Guest (s) init
[14:36:59] GM: 1 Module(s) init
[14:36:59] GM: 2 Tab (s) init
[14:36:59] RSTD.Client_LoadXml()
[14:36:59] [RadarAPI]: ar1.selectRadarMode(0)
[14:36:59]
[14:36:59] &&&&&&&&&&&&&&&&&&&&
[14:36:59] ***Script FAILED!***
[14:36:59] &&&&&&&&&&&&&&&&&&&&
[14:36:59] Exception message is:
[14:36:59] Unable to load DLL 'RadarLinkDLL.dll': The specified module could not be found. (Exception from HRESULT: 0x8007007E)