This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: I need to reboot MMWCAS-DSP-EVM to boot up MMWCAS-RF-EVM automaticly.

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: MMWCAS-DSP-EVM,

Hi supporter:

We set the  MMWCAS-DSP-EVM to boot up and load firmware MMWCAS-RF-EVM automaticly.

But sometimes the MMWCAS-RF-EVM can`t boot up,and I need reboot  MMWCAS-DSP-EVM manually. Then MMWCAS-RF-EVM can work property.

Do you have any comments about this ?

thanks~

  • Hello User,

    I'm not sure if I understood your query right.

    As soon as you supply power to the MMWCAS-DSP-EVM, do you see the MMWCAS-RF-EVM bootup? If that is not the case then please check the connection between both the boards (on the connectors). It is recommended to connect both the boards end to end (all four corners using the supports provided)

    Secondly, are you able to use mmWave studio with the setup? 

    Regards,

    Ishita