Hi,
In the "Interference MItigation for AWR/IWR devices" app note, section 3.3 Sense & avoid, I feel there is some contradiction in the explanation.
> One, it mentions for this approach we have to keep Tx off & Rx ON to receive any info from other transmitting devices
>Two, Both in figure 7 and the description above it, it is mentioned that the fast chirps of 250MHz/us should be used to scan the area for interference.
I think these two are contradictory.
Should I consider them as two different approaches?
Thanks in advance
-Santhana Raj