Other Parts Discussed in Thread: MMWAVE-SDK, AWR1443, UNIFLASH
Hi Team,
Our customer is looking for the xwr14xx_mmw_demo.bin file in MMWAVE-SDK_02.00.00.04. Upon checking the MMWAVE-SDK_02.00.00.04 from the two download links below, I noticed that the file sizes are different for the same version, 312836K vs 305505K. Please refer to the SDK in the links below.
software-dl.ti.com/.../index_FDS.html
We can't install the SDK to our computers so we can't verify the content of the files. Please confirm if the xwr14xx_mmw_demo.bin are available in the SDK.
Here are additional inquiries from the customer.
For correct operation of mmWave SDK demos, this utility needs 2 binary images:
BSS : mmwave_sdk_<ver>\firmware\radarss\xwr12xx_xwr14xx_radarss.bin
MSS : For the SDK packaged xWR14xx demos and ccsdebug utility, there is a bin file provided in their respective folder
For demo mode, choose the binary file mmwave_sdk_<ver>\packages\ti\demo\xwr14xx\mmw\xwr14xx_mmw_demo_mss.bin from the SDK
I want to find the xwr14xx_mmw_demo_mss.bin file in in MMWAVE-SDK_02.00.00.04 not the other version
There is no such path " mmwave_sdk_<ver>\packages\ti\demo\xwr14xx\ " in my sdk files...
I couldn't flash the xwr14xx_mmw_demo.bin file which is in MMWAVE-SDK_02.01.00.04 to my evm
Now I have three sdk versions which are 1.2, 2.0, 2.1
I can only run the demo in 1.2 version.
This is the screenshot of the error while I tried to flash the only xwr14xx_mmw_demo.bin file to the evm
I know that two bin files should be flashed to the evm in sdk 1.2 but the user guide of sdk 2.1 said I only need to flash one file
Regards,
Danilo