Hello,
Are there any guidelines for properly using "rlRfSetLdoBypassConfig()"?
- Can we call the above API at any point during the sensor configuration before the sensor is started?
- Can the above API be called from any core? (MSS or DSS)
- Do we have to have some amount of sleep/delay after calling the above API?
Other than setting the correct PMIC voltage rails, is there anything else we should be aware of when setting the LDO configuration for 1.3V or 1.0V operation? Anything in addition to the ICD?
Thanks,
Erik