Other Parts Discussed in Thread: UNIFLASH, AWR1243BOOST, AWR1843, AWR2243
Hi,
We have a customer with below concern:
I am aware of the serial flash in the AWR2243BOOST, however, all what I need to know if it is possible to load the firmware on the serial flash without using the mmWave studio and the DCA1000? or at least just without using the mmWave studio??
So, my question is simple, I just wanna know if the AWR2243BOOST can be flashed without connecting the board to the mmWave studio?
I tried using the UNIFLASH tool following the steps mentioned in the SDK guide. However, using the UNIFLASH tool I succeeded in erasing the serial flash when trying to flash the RSS and MSS image it fails, and the board is mentioned as unrecognized hardware.
The SDK guide never mentions any information about the AWR2243BOOST or at least the AWR1243BOOST, nor, based on what I've seen, have a sample code for such boards. The SDK guide is mainly focused on programmable boards like AWR1843. If I'm missing something, please show me where to find such a demo in the SDK.
Regards,
Roland