Other Parts Discussed in Thread: AWR2243
What is the correct API to configure a chirp based or frame based phase configuration on AWR2243BOOST?
I am using the following and the getting this error:
[RadarAPI]: ar1.SetPerChirpPhaseShifterConfig(0, 0, 0, 0, 37)
Status: Failed, Error Type: API IS ISSUED FOR AN UNSUPPORTED DEVICE
Chirp Based Phase Shifter Configuration #1 failure
Here are tha board spec:
HW: AER2243BOOST
DATA: DCA1000
MSSFwVersion:(02.02.02.00 (29/07/20))
BSSFwVersion:(02.02.00.13 (07/03/20))
BSSPatchFwVersion:(02.02.02.06 (12/08/20))
GUI: 3.0.0.14
FPGA Version: 2.8 [Record]