This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Why the antPhaseRot setting for IWR6843AOP is different in 3D ppl and overhead ppl?

Part Number: IWR6843AOP


Hi,

I found the antPhaseRot setting for IWR6843AOP is different in 3D ppl and overhead ppl. Would you pls kindly advise why?

C:\ti\mmwave_industrial_toolbox_4_6_0\labs\people_counting\68xx_3D_people_counting\chirp_configs\AOP_6m_default.cfg

antPhaseRot 1 -1 1 -1 1 -1 1 -1 1 -1 1 -1

C:\ti\mmwave_industrial_toolbox_4_6_0\labs\people_counting\overhead_3d_people_counting\chirp_configs\pc_6843_3d_aop_overhead_3m_radial.cfg

antPhaseRot -1 1 -1 1 -1 1 -1 1 -1 1 -1 1

I checked the 3.3.2. Antenna Phase Rotation Configuration of 3D_people_counting_detection_layer_tuning_guide.pdf, but I am still not clear how to set antPhaseRot. Would you pls kindly explain more?

  • Hi Chris,

    Those two commands are actually equivalent to each other. Since it is saying ant 0 and 1 have a phase shift from eachother, it doesn't matter whether the negative is in the ant0 or ant1 position.

    This antPhaseRot parameter is fixed by the antenna design, so should not need to be reset for any of the EVMs.  In the detection layer tuning guide, it suggests to use the below config for AOP, but both are equivalent.

    antPhaseRot -1 1 -1 1 -1 1 -1 1 -1 1 -1 1

    Regards,

    Jackson