This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: AWR1243P test source issues

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: AWR2243

Hello,

I am using the TI AWR1243P cascade board with the MMWCAS-RF-EVM (Rev-E) connected to the MMWCAS-DSP-EVM.

mmWave studio software: version 02_01_01_00

Firmware: mmwave_dfp_01_02_06_03

I followed the steps in the user guide to run the test source file.

The default settings in "Cascade_Configuration_TestSource.lua" and "Cascade_Capture.lua" . I have only updated the capture directory, the metafile path, and the IP address in these LUA scripts. 

After I transfer the files and post-process, I get the following plots.

From what I understood in "Cascade_Configuration_TestSource.lua" script is that we have two test sources (objects) at 5m and two test sources (objects) at 13m. Each object is defined for one device.

The postprocessing plots do not display these four objects. Any idea how can I fix this? thank you.

Post processing plots of the test source