Hello Champs,
IWR6843AOP ES2.0 +mmwaveicboost
industrial toolbox: 4_6_0
Ubuntu 16.04 LTS
Configure iwr6843aop SOP to be mmwaveicboost boot mode and set mmwaveicboost sop2 to OFF and set S1, S2, S3 as shown in Figure 4-15. Switch Configuration for MMWAVEICBOOST Mode in https://www.ti.com.cn/cn/lit/ug/swru546d/swru546d.pdf.
When running roslaunch, the grid can be opened, but there is no point cloud and it prompted below error:
[ERROR] [1618568607.619879676]: mmWaveQuickConfig: Command failed (mmWave sensor did not respond with 'Done')
[ERROR] [1618568607.619941001]: mmWaveQuickConfig: Response: ''
Thanks.
Rgds
Shine