This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP422-Q1: Question for the setting of "two-Wire Interface Slave Device Addresses"

Part Number: TMP422-Q1
Other Parts Discussed in Thread: TMP422

Hi

We have a design issue for the device addresses of TMP422-Q1 setting.

Setting following.

We design it for I2C address "1001 111"(0x4F), but the device addresses is "1001 110"(0x4E) that we detect.

DX3 and DX4 connect to arria 10 device(10AX032E).

Do you have any suggestion for this?

Best Regards

Frank