This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP144EVM: adding additional TMP144 ic's to the evm

Part Number: TMP144EVM
Other Parts Discussed in Thread: TMP144,

Hello

Can we add additional TMP144 ICs to the chain. If yes then are they readable in the GUI. 

Also Can we export the temperature data from the GUI?

Thank you

Varun

  • Hi Varun,

    Thank you for your post. 

    Can we add additional TMP144 ICs to the chain. If yes then are they readable in the GUI. 

    You can add additional TMP144 ICs to the chain, but they will not be readable in the GUI, the GUI composer framework cannot handle a variable number of devices. 

    Also Can we export the temperature data from the GUI?

    The current version of the TMP144EVM GUI does not support data logging.

    Best Regards,
    Brandon Fisher