Other Parts Discussed in Thread: AWR1443
Greetings,
I am currently playing with AWR1443 + mmWDevPack + TSW1400, and I am following the tutorial at [mmWave_sensor_raw_data_capture_using_TSW1400_board_v3.pdf]. Apart from cannot format AWR1443, I also met the problem the mmWave 2.1.1.0 IDE is buggy, I cannot see the output logs windows. Whether I (1) click run `DataCaptureDemo_xWR.lua` it does not show anything (2). I follow `Capturing the radar data` section in the slides. I get nothing.
1. I get HSDC installed and load in the correct firmware
Can I have older version like Radar Studio version 1.6.2. as shown in the slides? Or could it be the conflict 2.1.1.0 with 3.0.0.14 since I also use cascade mmW.
Best
Jet