This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843ABL

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843, , DCA1000EVM

Dear TI,

 Is there any provision for separate chip(debugger) for flashing the code via USB for AWR1843? If so, our company is planning to use it in production. May I know the chip number, IC number, relevant software used and license to be followed.

  • Flashing to AWR1843 device requires UART connection. You can use any UART-to-USB chip which emulates UART to COM port for this purpose instead of XDS110 which is available on AWR1843BOOST.

    XDS110 or FTDI chip which is used on AWR1843BOOST and DCA1000EVM, can be used to emulate UART connection to the PC.

    But there are other ICs also in the market which you can go for.

    .

    Regards,

    Jitendra