Hi Team,
My customer design TDC7201 and their clock value is limited.
From specification, The System clock of TDC7201 is 8 Mhz by default, and the maximum support is 16 MHz.
Now if customer only can provide the System clock is 14.286 Mhz (714.286 = 100/7 ), so question is
(1) Does TDC7201 support 14.286 Mhz?
(2) When the FW is used under the system clock synchronization setting of 14.286 Mhz, will it affect the accuracy?
(3) Besides clock value, is there any other specification customer need to pay attention?
Thanks