This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: unresolved ticket in industrial toolbox

Genius 9880 points
Part Number: IWR1843BOOST


Hi Team.

We have received inquiry regarding the  mmwave_industrial_toolbox. Below is the customer inquiry.

"

I am working on combining a customized Data Processing Chain based on mmwave_industrial_toolbox_4_6_0 labs and demos from mmwave_sdk_03_05_00_04.

In this processing chain, I need pointcloud data in spherical format for object tracking. I noticed /* @TODO MMWAVESDK-1868:BEGIN */ tags in industrial toolbox code. The tags appear specifically in places related to point cloud spherical data. Should I be concerned about the functionality? What is the underlying issue?

Additionally, there is separate AoA processing DPU hardware implementation in the toolbox (labs/common/src/dpu/aoaproc/aoaprochwa.*), which also has previously mentioned ticket tags. Although it doesn't seem to be included or used anywhere in the toolbox. Is it actually usable?

I have also reviewed the latest version (4.7.0) of the toolbox which has the same properties.

"

Thank you in advance.

Regards,

Maynard