This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Host MPU Recommendation for AWR2243

Part Number: AWR2243

Hi 

Could you please recommend appropriate MPU device which can be interfaced with AWR2243. 

According to AWR2243 related document, it introduced Jacinto device. TDA. But it can be heavy device to handle by customer application sometimes.

Is there any other alternative MPU to support AWR2243 among Sitara/DSP series or new device from Jacinto?

Thanks. 

  • These are the requirement for MPU selection to interface with AWR2243.

    1. It should have 4-line SPI and few sets of GPIO (HostIRQ , nReset, SOP control). 

    2. CSI-2 interface to capture raw ADC data from AWR2243 device.

    3. Signal Processing capability (DSP) to process received raw ADC data from AWR2243 device.

    So based on these requirement you can select the processor as per your usecase need.

    Regards,

    Jitendra