This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01000: Integration of TIDEP-01000 as a safety control

Part Number: TIDEP-01000


We currently have a Palomat conected to a conveyor on line, the operator access this area to remove the empty pallets after they add up. We also have a laser curtain sensor to prevent the machine from moving while there is an operator in that area, the problem is that once the operator is behind that laser line the machine can't detect the person and might start again. Also we want to make sure that the operator (for good or bad reason) will step in the palomat and at the same time I don't want the palomat to stop because it detected something other than a human.

This is why I am wondering if we can integrate your mmWave sensor in our production line.