Hi,
My customer manufactured AWR2243 custom board.
They found a issue on PCB that 1.8V power supply was not connected to VIN_18BB pin.
- Before fixing the issue, they want to use the board for evaluating SPI communication.
- They tried to boot the board and sent some SPI commands to AWR2243, the SPI communication was working for a while, and then corrupted.
- It is not possible to use SPI/UART/etc. without VIN_18BB power supply?
- Which blocks in AWR2243 is powered by VIN_18BB?
Thanks,
-Shibata