Part Number: AWR1243
Other Parts Discussed in Thread: , IWR1443
Hello,
My customer is wants to start develop a product based on several AWR1243 chips
Regarding about their design and architecture they going to use cascading multiple devices and design their own antenna array.
To achieve this they will need assistance in the following :
- Understand the phase difference per channel when transmitting from each device so they can calculate and interconnect with multiple devices?
- What the total phase difference in LOin versus LOout per device (AWR1243)?.
This documents http://www.ti.com/lit/wp/spyy007/spyy007.pdf doesn't fully answer their questions and if you can provide from the business unit Reference Design for such deployment of three or four AWR1243 in cascading multiple devices design it’s very important (If NDA process is needed there is no problem doing so)
3. What are the maximum salves in cascade mode ? if we can cascading more than 4 in parallel (1 master and 3 slaves)?
4. What is the BIT resolution of the CSI-2 interface (12/14/16 bit)?
5. There is any documentation of how heat dissipation of the device (AWR1243)?
6. Can the TSW1400evm support to 2 units of AWR1243BOOST simultaneously ? (it has 8LVDS lanes what about 2 separate clocks) and if Altera FPGA firmware is open ?
7. Is there an OrCAD alternative of schematics of AWR1243BOOST ?
If you can answer my questions, I will really appreciate it.
Thank you for your time effort
Best Regards.
Shai Berman