Other Parts Discussed in Thread: AWR1243BOOST, AWR1642BOOST
Hi,
I am working with the AR1443EVM-010 (XAR1243 Chip) in combination with the AR1XXXEVM-012 and the TSW1400.
The TI-Software I'm using: Radar Studio Ver: ar1: 1.6.1.0 and HSDC Pro v4.50
So until now mostly everything worked just fine, but now I'm stuck trying to start a measurement using the Hardware Trigger.
So here's what I do:
About the Hardware Setup:
All three boards are connected to each other.
Additionally I connect the output of a signal generator (50ohm) to the Pins J4.9: (40PIN_SYNC_IN) and J4.4 (GROUND) of the AR1XXXEVM-012 via a 30cm coax-cable
V_pp on the signal generator is set to 3V3. The function is a square with a frequency of 1Hz.
About my software-settings:
I use the folloing settings in the AdvFrameConfig in Radar Studio.
The HSDC Pro is set just as if I was using the Software Trigger.
Using the Softwaretrigger starting a measurement form the Sensor Config everything is working just fine with these settings. When I’m trying to use the HW-Trigger, there is no reaction after any signal edge.
I was also tring to use the mmw_demo.exe in HW-Trigger mode. Also no reaction here on my signal.
Any ideas where I went wrong?
I'm looking forward for your ideas.
If you're missing any Information, please tell me!
Best regards
Konstantin