Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642, UNIFLASH
Hi,
I am trying to run the demo visualizer on my AWR1642BOOST but I am having problems. The complete output from the console is:
mmwDemo:/>% *************************************************************** Skipped mmwDemo:/>% Created for SDK ver:01.01 Skipped mmwDemo:/>% Created using Visualizer ver:2.0.0.0 Skipped mmwDemo:/>% Frequency:77 Skipped mmwDemo:/>% Platform:xWR16xx Skipped mmwDemo:/>% Scene Classifier:best_range_res Skipped mmwDemo:/>% Azimuth Resolution(deg):15 Skipped mmwDemo:/>% Range Resolution(m):0.044 Skipped mmwDemo:/>% Maximum unambiguous Range(m):9.02 Skipped mmwDemo:/>% Maximum Radial Velocity(m/s):1 Skipped mmwDemo:/>% Radial velocity resolution(m/s):0.13 Skipped mmwDemo:/>% Frame Duration(msec):100 Skipped mmwDemo:/>% Range Detection Threshold (dB):15 Skipped mmwDemo:/>% Doppler Detection Threshold (dB):15 Skipped mmwDemo:/>% Range Peak Grouping:enabled Skipped mmwDemo:/>% Doppler Peak Grouping:enabled Skipped mmwDemo:/>% Static clutter removal:disabled Skipped mmwDemo:/>% *************************************************************** Skipped mmwDemo:/>sensorStop Done mmwDemo:/>flushCfg Done mmwDemo:/>dfeDataOutputMode 1 Done mmwDemo:/>channelCfg 15 3 0 Done mmwDemo:/>adcCfg 2 1 Done mmwDemo:/>adcbufCfg -1 0 0 1 0 Error: Invalid usage of the CLI command Error -1
I am using SDK 1.1
I was also trying to use other SDK versions but system just allow me to use SDK 1.1.