Part Number: AWR1243
Other Parts Discussed in Thread: UNIFLASH,
Hi,
I am trying to use Uniflash to load the firmware using the RS 232 lines on the AWR1243P chip (Custom board from a customer). When I connect the the Uart lines, It gets successfully detected in the Device manager.
But the problem is that Uniflash is not able to initialize the COM port, while trying to flash the device.
Hence my questions are as below:
1) Is it correct way to expect using UART lines of AWR1243P to flash firmware using Uniflash? We dont have any Ftdi chip on the custom board.
2) If yes, to the above question, is there any areas that I should debug, to find out the root cause of why I am not able to detect COM port properly in Uniflash??
3) Should there be some basic firmware already running on the chip to use Uniflash? or the boot loader is enough to carry out this process?
4) As explained in previous related question, We have a previous version of hardware, in which this approach to flash firmware using Uniflash used to work. In the current version it does NOT. Is it related to AWR1243 (old board) to AWR1243P(new board) changes in the hardware chip?
Any help on this issue, would be really helpful.
Thanks in Advance,
Santhana Raj